MPC5777C EBI SRAM interface

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5777C EBI SRAM interface

51,206 次查看
Boopathy_Rangaraj
Contributor II

Hi,

I'm working with MPC5777C in S32DS, I'm trying to interface SRAM (Flow through Burst) using EBI. Here i have initialized all the given EBI registers as per the reference manual. Still EBI is not generating any signals, all EBI pins are in pulled high state. I couldn't able to resolve the issue as there is no reference for EBI interface in S32DS.

Is there any component library or driver file for EBI(MPC5777C), or kindly provide any initialization steps for EBI.

Herewith attached my program.

标记 (2)
0 项奖励
回复
7 回复数

51,182 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, at first glance I see an error in your code, writing 2 times to the same register (it should be BR and OR registers). The values it indeed wrong.

davidtosenovjan_0-1644919355048.png

Here you may find example code for external SRAM used on MPC5777CEVB (it uses GHS compiler, but all settings you can find in main file):
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-External-SRAM-test-GHS714/ta-p/...

Also pay attention to following bullettin, section 5:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/External-Bus-Interface-FAQs/ta-p/1124068

 

 

 

 

0 项奖励
回复

51,177 次查看
Boopathy_Rangaraj
Contributor II
#include "MPC5777C.h"
#include "stdio.h"

#define SDRAM_BASE 0x20000022

  static void User_HW_init(void)
  {
      /* set round robin for all slaves */
      XBAR->PORT[0].CRS = XBAR_CRS_ARB(1);
      XBAR->PORT[1].CRS = XBAR_CRS_ARB(1);
      XBAR->PORT[2].CRS = XBAR_CRS_ARB(1);
      XBAR->PORT[3].CRS = XBAR_CRS_ARB(1);
      XBAR->PORT[4].CRS = XBAR_CRS_ARB(1);
      XBAR->PORT[6].CRS = XBAR_CRS_ARB(1);
      XBAR->PORT[7].CRS = XBAR_CRS_ARB(1);

  }

  void External_SRAM_MMU_init(void)
    {

        __asm__("e_lis    %r3,0x1002");      // Select TLB entry#, define R/W replacment control
    	__asm__("mtspr    624,%r3");        // Load MAS0 with 0x1002_0000 for TLB entry #2

    	__asm__("e_lis    %r3,0xc000");      // setup 512MBytes to cover the whole EBI space
    	__asm__("e_or2i   %r3,0x0980");          // TLB valid, protected from invalidation
    	__asm__("mtspr    625,%r3");        // Load MAS1 with 0xC000_0980 for TLB entry #2

    	__asm__("se_bgeni %r3,2");           // virtual address at 0x2000_0000
    	__asm__("e_ori    %r3,%r3,0x0038");   // VLE, cache-inhibited, write through
    	__asm__("mtspr    626,%r3");        // Load MAS2 with 0x2000_0038 for TLB entry #2

    	__asm__("se_bgeni %r3,2");           // physical address at 0x2000_0000
    	__asm__("e_ori    %r3,%r3,0x003f");   // all accesses permitted
    	__asm__("mtspr    627,%r3");


    	__asm__("msync");          // make sure we finished all memory accesses
    	__asm__("tlbwe");          // Write entry defined in MAS0 (entry #2 here) to MMU TLB
    	__asm__("se_isync");       // Wait for tlbwe to complete, then flush instruction buffer
    }


  static void External_SRAM_init(void)
  {
  	volatile unsigned int count = 0;

      /* Change EBI Physical Base Address to 0x2000_0000 */
      External_SRAM_MMU_init();


      /* CLKOUT Divide by 4 -> 33MHz          */
      SIU->ECCR = 0x00001003;

      SIU->PCR[256] = 0x0443;

      /* CS0                    PCR 256       */
      SIU->PCR[256] = 0x0443;

      /* D_ADD_DAT31            PCR 257       */
      SIU->PCR[257] = 0x0840;

      /* D_ADD_DAT16 - 30       PCR 263 - 277 */
      for (count = 263; count <= 277; count++)
      {
          SIU->PCR[count] = 0x0443;

      };

      /* D_ADD_DAT0 - 15        PCR 278 - 293 */
      for (count = 278; count <= 293; count++)
      {
          SIU->PCR[count] = 0x0440;
      };

      /* D_RD_WR                PCR 294       */
      SIU->PCR[294] = 0x0443;

      /* D_WE0 - D_WE1          PCR 295-296   */
      SIU->PCR[295] = 0x0443;
      SIU->PCR[296] = 0x0443;

      /* D_OE                   PCR 297       */
      SIU->PCR[297] = 0x0443;

      /* D_TS                   PCR 298       */
      SIU->PCR[298] = 0x0443;

      /* D_ALE                  PCR 299       */
      SIU->PCR[299] = 0x0443;

      /* D_TA                   PCR 300       */
      SIU->PCR[300] = 0x0443;

      /* D_CS1                  PCR 301       */
      SIU->PCR[301] = 0x0443;

      /* D_BDIP                 PCR 302       */
      SIU->PCR[302] = 0x0443;

     // SIU->PCR[307] = 0x0443;

      /* D_WE2 - D_WE3          PCR 303 - 304 */
      SIU->PCR[303] = 0x0443;
      SIU->PCR[304] = 0x0443;

      /* D_ADD9 - D_ADD11       PCR 305 - 307 */
      for (count = 305; count <= 307; count++)
      {
          SIU->PCR[count] = 0x443;
      };

      /* D_ADD12 - D_ADD15       PCR 259 - 262 */
      for (count = 259; count <= 262; count++)
      {
          SIU->PCR[count] = 0x0443;
      };

      /* Base Address: 0x20000000, 16-bit, non-Mux'd bus */
      EBI->CAL[0].BR = 0x20000001; //burst access

      /* Address Mask: 512KBytes, Zero Wait States -  Flow-Through Sync SRAM */
      //EBI->CAL[0].OR = 0xfff80012;
      /* Address Mask: 512KBytes, One Wait States - Pipelined Sync SRAM */
      EBI->CAL[0].OR = 0xFFF80010;

      /* MCR - 32-bit mode */
      EBI->MCR = 0x00000801;

  }



/*! 
  \brief The main function for the project.
  \details The startup initialization sequence is the following:
 * - startup asm routine
 * - main()
*/
int main(void)
{
  /* Write your local variable definition here */
int i = 0;


volatile uint32_t *sdram = (uint32_t*)SDRAM_BASE;
  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
  #ifdef PEX_RTOS_INIT
    PEX_RTOS_INIT();                   /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of Processor Expert internal initialization.                    ***/

  /* Write your code here */
    CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
                                  g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
    CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);

    User_HW_init();

    External_SRAM_init();


    for(;;)
         {

    	*sdram = (uint32_t)0x1234;
}
}

Thanks for your reply.

Yes, later I changed the register configuration now I'm able to write in SRAM.

But, when i tried to write in a particular location data is being written in all locations.

And also unable to write data in Muxed 32 or 16 bit.

refer the following attachments.

thanks in advance.

标记 (3)
0 项奖励
回复

51,159 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Which is used memory? Your connection? If it is flow through, as you said, you should use zero wait state (commented out in the code)

If you see the same value in all fields, in indicates an issue with addressing.

0 项奖励
回复

51,155 次查看
Boopathy_Rangaraj
Contributor II

Memory I'm using is CY7C1471BV33-133BZI (cypress). Hardware connections are  as it is in the uploaded schematic previously.

Yes, the memory is a flow through burst synchronous, also I used zero wait states configuration which is commented in the example program.

For addressing in SRAM there are 2 pins which is A0 and A1 field select and A(address) pins, I tried all the possible combinations, still data is being written in all the fields.

But in Muxed 32 and 16 bit data is not even written in single address. I didn't understand what I'm missing here. 

标记 (2)
0 项奖励
回复

51,134 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Does this mean you only have connected five address lines? Why there is a latch device there, if unconnected? Please explain

davidtosenovjan_0-1645112715812.png

 

0 项奖励
回复

51,100 次查看
Boopathy_Rangaraj
Contributor II

As per my application I want to use 16 bit or 32 bit muxed mode. So, latch is used and also usage of latch is mentioned in datasheet. My major doubt is whether the connections are fine or else I need to do some changes. 

In non mux mode I can able to write data but instead of being written in specific location, it is written in complete CS0 address range locations. 

I'm only confused on the address pins connection. We did the connection same as evaluation board (MPC5777c daughter board). The only difference is SRAM which is interfaced CY7C1471BV33-133BZI for more memory.

0 项奖励
回复

51,083 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

You haven't answered my question.

On the screenshot it seems on the memory side only address lines A_0, A_7, A_8, A_13, A_14 are connected what's wrong, of course, if it is so.

0 项奖励
回复