MPC5777C: Does the CMU_2 would affect the e2eECC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C: Does the CMU_2 would affect the e2eECC?

659 Views
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

 

On RM, CMU_2 is used for Crossbar, Memories and Flash Controller, etc. ECC also covers some of them. If CMU_2 detect faults and report to FCCU, does it also can cause the e2eECC error report? If yes, how?

<![if !vml]>

hongpingxu-b364_0-1613709072029.png

 

<![endif]>

hongpingxu-b364_1-1613708253130.png<![if !vml]>

hongpingxu-b364_1-1613709072378.png

 

<![endif]>

hongpingxu-b364_0-1613708091339.png 

Best regards,

 

Hornby

0 Kudos
3 Replies

639 Views
hongpingxu-b364
NXP Employee
NXP Employee

Hi,

My customer reported that they got their customer return.

When they duplicate the problem, they find that FCCU will report CMU_2 errors, and most of the time RAM ECC will report errors at the same time, so the customer wants to confirm whether the two are related?

Best regards,

Hornby

0 Kudos

603 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I see.

If CMU monitors clock source for the memory as it is in this case, then it is apparently possible. I would expect bus error in such case when stable clock is not provided to to memory module.

 

0 Kudos

648 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I am afraid I don't see any relation between CMU and e2eECC. Could you specify the question more in detail?

0 Kudos