MPC5777C Checker core

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C Checker core

1,359件の閲覧回数
darq
Contributor III

Hello,

Is there any documentation on checker core of MPC5777C? What does it do exactly? What are the results of its operation and when? Reference manual seems very limited in this regard.

Best regards

0 件の賞賛
返信
3 返答(返信)

1,343件の閲覧回数
darq
Contributor III

Thank you for your answers.

One last thing that i would like to have clarified is when are specific faults set in FCCU? I assume only fault 10 (RCCU_0) and fault 11 (RCCU_1) are valid for checker core? When is each of them set because description for both of them is the same: "Safety cores out of sync during lockstep. Fault is cleared by clearing the FCCU channel status, FCCU_NCF_Sn[NCFSm]."

Best regards

0 件の賞賛
返信

1,347件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, that is basically it. As a user you have access to safety core outputs via FCCU and RCCU.

Only configuration you can do is to enable/disable LSM and to set reaction on fault.

It is only replicating the main core execution. Once there is a mismatch in comparison it will notify the device.

 

best regards,

Peter

0 件の賞賛
返信

1,356件の閲覧回数
Varshap
Contributor I

The MPC5777C is ASILD MCU, its safety core operates in delayed lockstep mode (LSM) to allow the highest safety level to be reached. The checker core will receive all inputs delayed by two clock cycles. Outputs of the checker core will be compared with outputs of the master core. Any differences will be flagged as an error and processed by the FCCU.

 

check for document  - Safety Manual for MPC5777C

0 件の賞賛
返信