MPC5777C CSE Boot MAC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C CSE Boot MAC

ソリューションへジャンプ
1,476件の閲覧回数
jeffcampbell
Contributor III

Quick question on the CSE - in the manual in the section for Secure Boot, it say that the MAC calculated over the secure boot region is compared with the stored BOOT_MAC, and if the stored value is zero, the new MAC is stored there instead.  If the secure boot section were to be modified at some point, is it possible to overwrite the value stored in BOOT_MAC?

ラベル(1)
タグ(2)
0 件の賞賛
1 解決策
1,218件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to change the BOOT_MAC if secure boot section needs to be modified. But this assumes some conditions and there can be different scenarios. Please refer to the CSE App Note "AN4234-Using CSE" for detailed description. Particularly refer the "Section 2.10: Code flash update procedure" which discusses this question. There are also SW examples for this App Note. Please see example "D.1.2: Reprogramming of a programmed part".

Peter

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,219件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Yes, it is possible to change the BOOT_MAC if secure boot section needs to be modified. But this assumes some conditions and there can be different scenarios. Please refer to the CSE App Note "AN4234-Using CSE" for detailed description. Particularly refer the "Section 2.10: Code flash update procedure" which discusses this question. There are also SW examples for this App Note. Please see example "D.1.2: Reprogramming of a programmed part".

Peter

0 件の賞賛
1,218件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I have spoken to application team and looks like we need to ask design directly.

I will inform you as soon as I will get reply from design.

Peter

0 件の賞賛