MPC5777C  CMU output to signals to FCCU and INTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777C  CMU output to signals to FCCU and INTC

1,253件の閲覧回数
jongminna
Contributor III

Dear Everyone,

 

Most of all, Thanks NXP guys for quick answer.

NXP Engineers' answers are very helpful to me.

 

 

Question 1 : I want to implement clock monitoring for MPC5777C(3N45H)

So I've studied MPC5777CRM and I found useful section 19.13.4 CMU output signals to FCCU and INTC (809page).

However, I have additional question about them.

 

The output signals of the CMUs are connected to the FCCU and CMU Interrupts.

I want to know correlation between CMU ISR and FCCU.

In other words, I want to configure only the FCCU. I don't want to use CMU ISR.

Is it possible?

I worry that If I don't configure CMU ISR, FCCU also doesn't work well.

 

Question 2: How can I make Clock fault forcibly. such as loss of clock or lock of lock, so on.

I alreday know FCCU fault injection and I tested that works well. I want to know other method for validation of clock monitoring.

 

Please give me advice.

BR

JM.

ラベル(1)
0 件の賞賛
返信
1 返信

1,090件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

1) Yes, it is possible. CMU to FCCU routing is independent to interrupt controller.

2) Maybe you could connect EXTAL pin to ground for a while to initiate loss-of-clock. Loss-of-lock condition should be possible to inject by changing of PLL frequency software way.

0 件の賞賛
返信