MPC5777C CAN-FD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C CAN-FD

Jump to solution
1,664 Views
marcuslim
NXP Employee
NXP Employee

Hi,

From the RM, it states that MPC577C is able to support 2 channel of CAN-FD.  Please advice if it is complaint to ISO11898-1 2015, or which year is it complaint to?

 

Regards,

Marcus

0 Kudos
Reply
1 Solution
1,628 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, sure it is 11898-1:2015. Apologizing for typo.

MPC5777C with maskset 2N45H has M-CAN module of “non-ISO CAN FD”.
MPC5777C with maskset 3N45H has M-CAN module of “ISO CAN FD”.

SPC5777CK2... (maskset 2N45H) “non-ISO CAN FD” - probably no longer on the market
SPC5777CK3... (maskset 3N45H) “ISO CAN FD”

The screenshot you have shared is all related to 3N45H.
MCUs with optional field you have NOT higlighted, I haven't found on our web. I think it rather means MCUs without M-CAN module.

View solution in original post

5 Replies
1,653 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

MPC5777C devices of mask set 3N45H offers ISO Compliant CAN-FD.

The M_CAN performs communication according to ISO11898-1 (Bosch CAN specification 2.0 part A,B) and to Bosch CAN FD specification V1.0.

0 Kudos
Reply
1,644 Views
marcuslim
NXP Employee
NXP Employee

Hi David,

Thanks!  But is it 2015 specification ?  Customer needs this confirmation.

 

Regards,

Marcus

 

0 Kudos
Reply
1,637 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, all products compliant to ISO standard 11898-2:2015 should be called “ISO CAN FD”. Products implementing Bosch’s original protocol should be named “non-ISO CAN FD”.

MPC5777C with maskset 2N45H has M-CAN module of “non-ISO CAN FD”.
MPC5777C with maskset 3N45H has M-CAN module of “ISO CAN FD”.

0 Kudos
Reply
1,633 Views
marcuslim
NXP Employee
NXP Employee

Thanks David !

I suppose you meant compliant to ISO standard 11898-1:2015.

From DS, the part selection will be those highlighted:

 

marcuslim_0-1622192103171.png

 

Regards,

Marcus

0 Kudos
Reply
1,629 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, sure it is 11898-1:2015. Apologizing for typo.

MPC5777C with maskset 2N45H has M-CAN module of “non-ISO CAN FD”.
MPC5777C with maskset 3N45H has M-CAN module of “ISO CAN FD”.

SPC5777CK2... (maskset 2N45H) “non-ISO CAN FD” - probably no longer on the market
SPC5777CK3... (maskset 3N45H) “ISO CAN FD”

The screenshot you have shared is all related to 3N45H.
MCUs with optional field you have NOT higlighted, I haven't found on our web. I think it rather means MCUs without M-CAN module.