MPC5775K NCF[4] Can't be cleared during FCCU initiation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5775K NCF[4] Can't be cleared during FCCU initiation

1,064 Views
shijianyong
Contributor I

Hi 

      Our product use MPC5775K and FS6523. There is a boot failure  when the ambient temperature below -25℃。

      

      The initiation process stop at the while loop of FCCU_init() :

         FCCU_init()     while(FCCU.CTRL.B.OPS != 0x3)

      

      I tried to clear all NCF before config FCCU, but NCF[4] can't be cleared, and SSCM_STATUS.CERS is set and can't be clear by writing '1'.

        

      When ambient temperature goes above -25℃, there is no such issue.  

      

      

      

petervlna

0 Kudos
6 Replies

802 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

you wont be able to clear this NCF[4] until the SSCM is still reporting it via CERS bit.

MEMORY_DCF_SAFETY_ERR - Indication of fault during timing/repair configuration initialization by SSCM of different memories. Faults can be caused by parity or triple-redundant errors in loaded configuration data.

In other words, you have a mismatch in safety DCF client you have programmed into UTEST flash memory.

Please make sure your safety DCF clients are correct or use our calculator:

MPC57xx - DCF records 

https://community.nxp.com/docs/DOC-335523 

Peter

0 Kudos

802 Views
fu860925
Contributor I

MPC5744P,fccu,after FCCU_DRV_Init,inject  ncf[0],  PMC->FIR = 0x4U,when debug this line,Error : Error in ONCE status register during instruction execution.  why?

0 Kudos

802 Views
shijianyong
Contributor I

Hi Peter,

      We didn't change the default DCF configuration, nor add any DCF records.  

      When ambient temperature goes above -25℃, there is no such fault.   I guess the fault is caused by parity or triple-redundant errors when loading configuration data, but I don't know why it occurs only when temperature is under -25℃.

0 Kudos

802 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

Do you see this behavior on all samples or on just one?

Do you have your custom board or NXP evaluation board?

Peter

0 Kudos

802 Views
shijianyong
Contributor I

Hi Peter,

        We tested 10 samples, and 4 samples have this behavior.  We have evaluation board of MPC5775K. 

0 Kudos

802 Views
petervlna
NXP TechSupport
NXP TechSupport

hmm,

Could you share with me dump of your UTEST flash.

Because NCF4 is called on CERS set in SSCM. I would like to check user area of UTEST. There is no other possibility to trigger this fault except CERS bit.

Which cut of device are you using? 0N76P?

Peter

0 Kudos