MPC5775K FlexCAN Loopback module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5775K FlexCAN Loopback module

1,367 Views
lihongrun
Contributor I

Dear all:

    I'm using MPC5775K to test FlexCAN module now,but I have a lot of questions in the loopback mode,the datasheet said that The Rx CAN input pin is ignored and the Tx CAN output goes to the recessive state (logic '1'),does it means that after I transmit  a frame of data ,I should change the state of Tx from output to input? Thank you!!!

0 Kudos
Reply
1 Reply

1,288 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

You need not change the state of pins. The loopback mode is used for internal test, for example testing of receive/masking operation. FlexCAN behaves as it normally does when transmitting and treats its own transmitted message as a message received from a remote node. The ACK field is ignored so the message can be received normally.

In the loopback mode no message is visible on TX output, it goes to the recessive state (logic “1”).

BR, Petr

0 Kudos
Reply