hi colleagues,
please help to answer following questions for MPC5775E
1. It's configured to Parallel mode in factory and it cannot be changed.
2. This DCF record is not visible for user.
3. Yes, it can be overwritten (i.e. adding new record) and only the latest value will be considered.
4. Yes, the BOOT_MAC can be updated using standard SHE update protocol - it's updated in the same way as keys. You can calculate the CMAC offline (for example using binary/srecord file and OpenSSL) or you can let the hardware to calculate the CMAC (during development). But the BOOT_MAC must be updated manually via SHE update protocol.
The BOOT_MAC can be calculated and stored automatically only first time as required by SHE specification. Next time it needs to be updated manually.
5. No, CSE can't be updated.
6. SHE specification is sometimes helpful. Please check NXP sharepoint.
Regards,
Lukas