MPC574xG : questions about FlexCAN time stamp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC574xG : questions about FlexCAN time stamp

Jump to solution
1,557 Views
neojung
NXP Employee
NXP Employee

Hello Sir,

For the MPC574xG family's FlexCAN time stamp, I have several questions like below.

 

1. When I set the CAN_0.CTRL2.B.TIMER_SRC, free running timer did not increased, and I confirmed this on our EVB. I set this bit field in freeze mode. Is there anything that I missed?

2. What is exact meaning of "external time tick" which is described in CTRL2 TIMER_SRC bit field description? is it mean FXOSC? please let me know the details about "external time tick".

3. I can't find CAN_0.CTRL2.B.TIMER_SRC on Laughterbach peripheral register monitor (View--> peripheral). If my PER file is old, would you please share with me the latest PER file for Calypso 6M and 3M family?

4. It seems that only MPC574xG family's FlexCAN has TIMER_SRC bit field. Is it right? Cobra55 and Rainier don't have TIMER_SRC.

 

Hope to receive any feedback!

 

Best regards,

Neo

Labels (1)
0 Kudos
Reply
1 Solution
1,310 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Neo,

yes, I have received following...

"The external clock is given by PIT_RTI module channel no.14  and no.15 to FlexCAN modules 0/1/2/3 and 4/5/6/7 respectively.

This information is missing in RM., will be corrected in next RM revision.

Also this is a change in MPC5748G from cut 2 to cut 3."

BR, Petr

View solution in original post

4 Replies
1,310 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Neo,

I can confirm this behavior. I will try to find out more about this "external time tick" as the RM says nothing.

Attached is PER file I have, the CTRL2[TIMER_SRC] is included there.

BR, Petr

0 Kudos
Reply
1,310 Views
neojung
NXP Employee
NXP Employee

Hello Petr,

Do you have any update on external time tick description?

Best regards,

Neo

0 Kudos
Reply
1,311 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Neo,

yes, I have received following...

"The external clock is given by PIT_RTI module channel no.14  and no.15 to FlexCAN modules 0/1/2/3 and 4/5/6/7 respectively.

This information is missing in RM., will be corrected in next RM revision.

Also this is a change in MPC5748G from cut 2 to cut 3."

BR, Petr

1,310 Views
neojung
NXP Employee
NXP Employee

Thank you, Petr!

Best regards,

Neo

0 Kudos
Reply