MPC5748G have too large current in the Standby mode.

cancel
Showing results for 
Search instead for 
Did you mean: 

MPC5748G have too large current in the Standby mode.

227 Views
wenhongkui
Contributor II

I modified the example of Standby and added the PLL program.

The test findings are as follows:
1 the first power on the chip, the chip can normally enter the Standby mode, the current is normal.
2 MPC5748G can use the WKUP12 PIN to wake up to normally run. But the current will be larger when it comes to the Standby mode again. At this time the external oscillator is closed, but the core voltage is not closed.
3 STM wake-up is invalid if PLL is used, but it is normal when PLL is not used.

0 Kudos
1 Reply

115 Views
petervlna
NXP Employee
NXP Employee

Hi,

2 MPC5748G can use the WKUP12 PIN to wake up to normally run. But the current will be larger when it comes to the Standby mode again. At this time the external oscillator is closed, but the core voltage is not closed.

Hmm, try to shrink code as much as possible. Measure the current waveform to see where is the difference.

3 STM wake-up is invalid if PLL is used, but it is normal when PLL is not used.

As you can see the PLL module is not active in standy mode, so it can source clock to STM. Only PD0 peripherals are active.

pastedImage_5.png

regards,

Peter

0 Kudos