MPC5748G for sending and receiving package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G for sending and receiving package

1,620 Views
xy1904312
Contributor I

I tried the rmii_udp example project and made board send messages to PC.

But I have no idea how to let board receive messages from PC.

I followed mpc5748g-ethernet-demo-user guide.pdf to practice mpc5748g-ethernet-LWIP-udp.rar

That is from here as the attach file.

I didn't change codes in the project as well as the default IP & MAC.

Though it built in the board successfully, no message received when I used NetAsistant to send UDP packets. 

I tried to trace code by setting LEDs to check where is not executed in the program.

And found if (NetNIC_RevCheck()) cannot be access because the LED inside if cannot be traggled.

WHY the packets cannot be received and WHERE's wrong.

 

Hope someone gives help.

0 Kudos
Reply
0 Replies