MPC5748G Spread Spectrum

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G Spread Spectrum

2,426件の閲覧回数
nextsteve
Contributor III

Hi, I'm interested in trying out the spread spectrum feature of the MPC5748G PLL.

Wondering if there are reference register values available for STEPSIZE, STEPNO, etc. I could use to test quickly while I work through the equations.

Thanks,

Steve 

タグ(2)
0 件の賞賛
返信
4 返答(返信)

2,061件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I have created example SW for you.

My STEP is 250 and modulation frequency is 20kHz.

I have verified it with spectral analyzer. You can use it as a reference.

https://community.nxp.com/docs/DOC-334867 

Peter

2,061件の閲覧回数
nextsteve
Contributor III

That is awesome Peter, Thanks! 

0 件の賞賛
返信

2,061件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

We do not have reference example for frequency modulation.

You have to calculate STEPSIZE and STEPNO.

From my past experience I recommend you after calculation to use spectral analyzer for manual fine tuning.

Peter

0 件の賞賛
返信

2,061件の閲覧回数
nextsteve
Contributor III

Hi Peter, does STEPSIZE need to be non-zero? 

If so, then I don't see how the calc can possibly work because with a 40MHz crystal and modulation freq=10kHz --> STEPNO=2000. N would have to be >2000 for STEPSIZE to round to anything other than 0.

What am I missing?

Thanks,

Steve 

0 件の賞賛
返信