[MPC5748G] Question about lwip example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[MPC5748G] Question about lwip example

1,002件の閲覧回数
kmh48301
Contributor IV

Hi.

I'm trying to test lwip example.

But I can't see any response from my board.

I have checked the documentation of this example. (which is located in sdk path)

and "readme" file which is located in "chargen" folder.

 

I think IP address allocation is something wrong.

 

//this is sdk original setting

#define LWIP_PORT_INIT_IPADDR(addr) IP4_ADDR((addr), 192,168,0,200)
#define LWIP_PORT_INIT_NETMASK(addr) IP4_ADDR((addr), 255,255,255,0)
#define LWIP_PORT_INIT_GW(addr) IP4_ADDR((addr), 192,168,0,1)

1. Do i have to set the ipaddress to 192.168.0.200 as the smae with my board?

But in the sdk document :

"Select Internet Protocol Version 4 and click Properties; select Use the following IP address and configure the IP address and subnet mask. Configuration example: IP - 192.168.0.10, subnet mask - 255.255.255.0."

: I did this. but no working.

2.and in sdk document

: Basic functionality can be checked by pinging the board from the host PC: ping 192.168.0.200

>>> i think this is something conflicting with "1".

 

* I'm using telnet utility with window cmd as the "readme" file mentions. and

working in debug ram mode.

 

Thanks

Best regards

Phillip

 

0 件の賞賛
返信
0 返答(返信)