MPC5748G MII_Lite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G MII_Lite

1,141 Views
AROK
Contributor I

I'm looking for the setting to enable the MII_Lite mode of Ethernet controller on the Calypso.  COL, RX_ER and CRS signals are not available on our design.

 

I've found any information is MPC5748G_RM v3 about making  Ethernet controller ignoring theses signals.

Labels (1)
Tags (3)
0 Kudos
2 Replies

809 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

No ENET setting is needed. Just pins should be handled accordingly.

See chapter 2.1 “MII versus MII-Lite” of the AN4577; http://www.nxp.com/files/32bit/doc/app_note/AN4577.pdf

It is written for the FEC module, but can be reused on MPC5748G too.

BR, Petr

0 Kudos

809 Views
AROK
Contributor I

That true for the MPC564xB-C. 

With the Calypso,  the MAC is supposed to support MII_Lite. More than this when both ethernet controller are used the COL pin is no longer available because it used for the second MII bus.

Rem: I'm trying to get some answers from my contact at NXP

Regards

0 Kudos