Hello,
I wanted to switch from the PE Micro Universal FX Debugger to the ISystem IC5500. I tried to flash the elf-files I received by compiling an empty S32-Design Studio project created by the wizard.
When starting to download the files I get the following error:
Error in download(): E_FAIL: isystem.connect call failed. / Error 22: Can not start emulation. Check Vcc and clock source
The connection with the debugger was tested and is working properly. Vcc is at 12 V. The steps I took are the same as described here:
(except that I tried to use JTAG to flash and I choose the IC5500).
Regards,
Stefan