MPC5748G: How to blink LEDs from different cores?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5748G: How to blink LEDs from different cores?

1,220 次查看
davidanderle
Contributor II

Hello,

I'm trying to periodically blink 2 LEDs - one from the z4_0 (100ms) and one from the z2 core (2000ms). These LEDs are on PTI14 and PTI15. 

However, I find that only one of the LEDs is blinking at a time. If I pause the execution of one core, the other core's LED starts blinking and vice versa. It appears to me that there are some bus arbitration issues I'm not seeing.

I have tried using the SEMA42 driver based on the  sema_multicore_mpc5748g project, but it resulted in the same outcome and starting the codes from the debugger/standalone shows the same behaviour.

I have even written my atomic PIN toggling function here to ensure that the 2 cores are not accidentally overwriting each other's commands.

 

void Pin_Set(GPIO_Type *const port, const uint32_t pinIdx, const bool val){
  const uint32_t mask = 1ull << (15-pinIdx);
  const uint32_t mppdo = val ? mask : 0;
  const uint32_t portIdx = ((uint32_t)port - (uint32_t)PTA_BASE)/2;
  SIUL2->MPGPDO[portIdx] = (uint32_t)(SIUL2_MPGPDO_MASK(mask) | mppdo);
}

void Pin_Toggle(GPIO_Type *const port, const uint32_t pinIdx){
  Pin_Set(port, pinIdx, !(port->PGPDO & (1ull << (15-pinIdx))));
}

// Task called on CPU2 (z2)
void Task_Handler_z2(void){
  // Entered every 2000ms
  if(STM_DRV_GetStatusFlags(INST_STM0, 1)) {
    STM_DRV_ClearStatusFlags(INST_STM0, 1);
    STM_DRV_SetStartValueCount(INST_STM0, 0);

    SEMA42_DRV_LockGate(0, 0);
    if(SEMA42_DRV_GetGateLocker(0, 0) == (GET_CORE_ID() + 1)){
      Pin_Toggle(PTI, 14);
      SEMA42_DRV_UnlockGate(0, 0);
    }
  }
}

// Task called on CPU0 (z4_0)
void Task_Handler_z4_0(void){
  // Entered every 100ms
  if(STM_DRV_GetStatusFlags(INST_STM0, 0)) {
    STM_DRV_ClearStatusFlags(INST_STM0, 0);
    STM_DRV_SetStartValueCount(INST_STM0, 0);

    SEMA42_DRV_LockGate(0, 0);
    if(SEMA42_DRV_GetGateLocker(0, 0) == (GET_CORE_ID() + 1)){
      Pin_Toggle(PTI, 15);
      SEMA42_DRV_UnlockGate(0, 0);
    }
  }
}

void main_z4_0(void){
  // ... Init hardware and stuff
  for(;;){
    Task_Handler_z4_0();
  }
}
void main_z2(void){
  for(;;){
    Task_Handler_z2();
  }
}

 

 

Has anybody got any suggestions what's wrong with my setup?

Thanks in advance!

0 项奖励
回复
2 回复数

1,193 次查看
davidanderle
Contributor II

It turns out I was using the same STM module and was resetting the counter on both CPUs. Using STM0 on CPU0 and STM2 on CPU2 has resolved this issue. But I did look into the cross bar settings and may be useful knowledge in the future.

0 项奖励
回复

1,203 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

It could be caused by XBAR priority arbitration. You could to try to configure XBAR to set round robin for all slaves for both cores. 

0 项奖励
回复