MPC5748G Datasheet (Rev.3) - possible typo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G Datasheet (Rev.3) - possible typo

666 Views
carlvanwormer
Contributor II

In the Absolute maximum ratings, the notes are:

3. VDD_HV_FLA must be connected to VDD_HV_A when VDD_HV_A = 3.3V
4. VDD_HV_FLA must be disconnected from ANY power sources when VDD_HV_A = 5V

 

In section 4.2, Recommended operating conditions, the notes are:

If VDD_HV_A is in 3.3V range, VDD_HV_FLA should be externally supplied using a 3.3V source. If VDD_HV_A is in 3.3V range, VDD_HV_FLA should be shorted to VDD_HV_A.

 

 

Should the first part of the 4.2 note be:

"If VDD_HV_A is in 5Vrange, VDD_HV_FLA should be externally supplied using a 3.3V source" ?

 

 

 

Another note in the recommended conditions is:

If VDD_HV_A is in 5V range, it is necessary to use internal
Flash supply 3.3V regulator. VDD_HV_FLA should not be
supplied externally and should only have decoupling capacitor.

 

In Figure 2. Voltage regulator capacitance connection, the VDD_HV_FLA pin is shown as just connecting to a capacitor, bypassing the internal regulator, but no voltages are indicated.

 

It appears that there is some rule relating to this pin that has not been fully explained.  Is there more information on the problem that is being solved by these various instructions?

 

Thanks,
Carl

Labels (1)
0 Kudos
Reply
1 Reply

532 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Carl,

all the notes are correct, there's no typo.

1. If VDD_HV_A = 3.3V then short VDD_HV_A and VDD_HV_FLA.

2. If VDD_HV_A = 5V then don't connect VDD_HV_FLA to power source, use only decoupling capacitor.

The difference is that in 5V mode (VDD_HV_A = 5V) internal regulator is used for VDD_HV_FLA. In 3.3V mode, the VDD_HV_FLA must be supplied externally.

Regards,

Lukas

0 Kudos
Reply