MPC5748G DEVKIT CLKOUT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G DEVKIT CLKOUT

ソリューションへジャンプ
1,629件の閲覧回数
antleite2001
Contributor I

Hi All

I am trying to route CLKOUT_0 and CLKOUT_1 to PG7 and PG6 with no success.

Scopemeter connected between J3.13 (GND) and J3.14 (PG[6]) are in 3v3

Scopemeter connected between J3.13 (GND) and J3.16 (PG[7]) are in 3v3

Components

clock_manager Tab CLKOUT CLKOUT0 and CLKOUT1 are enabled

pin_mux PG[6] routed to Platform/clkout/1

PG[7] routed to Platform/clkout/0

Thanks in advance

 

Antonio Leite

0 件の賞賛
返信
1 解決策
1,596件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, have you checked pad configuration in the debugger whether it fulfills setting defined in the I/O excel?

davidtosenovjan_0-1649832188294.png

Also it is needed to have configured CLKOUT clock source and configured CLKOUT divider(MC_CGM_AC6_SC and MC_CGM_CLKOUT1_SC).

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,597件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, have you checked pad configuration in the debugger whether it fulfills setting defined in the I/O excel?

davidtosenovjan_0-1649832188294.png

Also it is needed to have configured CLKOUT clock source and configured CLKOUT divider(MC_CGM_AC6_SC and MC_CGM_CLKOUT1_SC).

 

 

0 件の賞賛
返信