MPC5748G CAN FD trace

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5748G CAN FD trace

631 次查看
JirikP
Contributor II

Hi, 

we are trying to implement multi CAN FD tracer. Is it possible to use Message buffer or any other option to receive all CAN FD messages without knowing their IDs?

 

Thanks

Regards Jiri

标记 (2)
0 项奖励
3 回复数

618 次查看
JirikP
Contributor II

Ok, thank you for your fast answer.

We are worried that when we receive one msg to MB that managing of the interupt and data would take too long and we would loose msgs in between. Is is possible to "daisy chain" the MBs or us DMA?

 

0 项奖励

614 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, this could happen, but it is already application problem, to read out MB in time.
DMA is only supported over RXFIFO, but RXFIFO cannot be used if CANFD is enabled.
You have option to use reception queue (MCR[IRMQ] set) by programming more than one MB with the same ID, received frame will be stored into first free-to-receive MB. Again refer to Matching process chapter.

BR, Petr

0 项奖励

623 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, it is possible. Use Mask acceptance register for it. If cleared incoming ID is don't care. Note by default IDE bit is always checked, but if CTRL2[EACEN] is set, the comparison of both Rx Mailbox filter’s IDE and RTR bit is enabled with their corresponding bits within the incoming frame and Mask bits do apply.
For more info refer to Matching process chapter of the RM and description of RXMGMASK and RXIMRx registers.

BR, Petr

0 项奖励