MPC5746R ECC ISSUE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746R ECC ISSUE

1,074 Views
曾经怀念
Contributor II

Can anyone give me a solution or documentation about ECC?

My current solution is

   Write different data to the same address and then read the address, this operation will trigger the IVOR2 interrupt, record the fault in the interrupt and clear the flag bit, exit the interrupt and erase the FLASH in the idle time.

    But C55FMC_MCR.EER cannot write 1 to clear, it will recover from 0 to 1.

And it's the same as MEMU.

Tags (2)
1 Reply

961 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, pay attention to following appnote, I have recently shared:

https://community.nxp.com/docs/DOC-339955 

It is written for MPC5744P, but several sections speak about MPC57xx overally.

 

Hope it helps