Hello,
I want to disable the weak pull up in each pad during Power on Reset or RESET.
In MPC5746R, weak pull up of all port are enabled as a default when it's POR/RESET.
After it's POR/RESET, I could disable the weak pull up by configuring the SIUL_MSCR[WPUE].
But, it need to be disabled when it's POR/RESET because it can cause the unwanted output.
Please share the solution if you have for this query.
Thank you.
Best regards,
Kimin
It seems it is just not possible to configure it before reset. I would recommend to install stronger external pull-down resistors for pins where it could cause issues to you.
I've also faced this issue on MPC5748G. Each reset causes ~100ns high pulse on GPIOs, so it is nightmare to debug code when these GPIOs are used to reset external peripheral or slave MCU...