MPC5746C SMPU - FMT1 Support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C SMPU - FMT1 Support

Jump to solution
1,488 Views
martinschulthei
Contributor III

Hello,

according to "Document Number: MPC5746CRM Rev. 4, 12/2016" the Calypso 3M derivatives no longer support the FMT1 Format for the System MPU. (Appendix A: Release Notes, General Changes "Removed "Region Descriptor n, Word 2 Format 1 (SMPU_RD_nW2_F1)" register" - page 3396).

Is this information correct for all Calypso3M derivatives ? Is there a mask set which supports FMT 1 ?

What about Calypso6M ? Will there be changes too ?

I need to ask because for our AUTOSAR OS we need to distinguish between Supervisor- and User Mode on memory access control. But from our point of view this isn't possible with this derivative if only FMT 0 is supported. Is this correct ?

Thanks in advance and best regards

Martin Schultheiß

Tags (2)
1 Solution
1,314 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I finally got an answer:

The changes to the RM with respect to FMT = 1 not now being supported are NOT correct. FMT =1 IS supported by both Cal 3M and Cal6M. There is an update to the reference manuals about to be released to reflect this.


Peter

View solution in original post

3 Replies
1,315 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I finally got an answer:

The changes to the RM with respect to FMT = 1 not now being supported are NOT correct. FMT =1 IS supported by both Cal 3M and Cal6M. There is an update to the reference manuals about to be released to reflect this.


Peter

1,314 Views
martinschulthei
Contributor III

Hi Peter,

thank u for the information. I'm glad to hear that.

BR

Martin

0 Kudos
Reply
1,314 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello Martin,

I have asked doc and apps team for clarification.

I will feedback you ASAP.

Peter

0 Kudos
Reply