MPC5746C ISO CANFD NOT WORKING

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5746C ISO CANFD NOT WORKING

835 次查看
akshay_hv
Contributor I

Hello,

I developed the CANFD driver for MPC5746C MCU . It is working fine CANOE if we select the NON ISO CAN FD option in CANOE tool.
But It is not working if we select the ISO CANFD. I tried to find information of configuring this in the code. I didn't find much information on this.

please clarify the point whether the micro will support ISO CANFD .. If so how to configure the same.

Regards

Akshay H V

标记 (2)
0 项奖励
回复
1 回复

718 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

be sure you are using the MCU with the maskset 0N84S or 1N84S. Those MCU cuts implements ISO CAN FD protocol.

Previous masksets are not compliant with ISO CAN FD, refer to erratas http://www.nxp.com/docs/en/errata/MPC5746C_1N06M.pdf.

BR, Petr 

0 项奖励
回复