MPC5746C AXBS PRS[7] and CRS[7] fail to read

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5746C AXBS PRS[7] and CRS[7] fail to read

521 Views
cholland
Contributor V

Hi,

The program locks up when I try to read  AXBS PRS[7] and/or AXBS CRS[7].

MGPCR[7] seems to work just fine, but the answer is always 0. (Perhaps its supposed to be 0?)

unsigned long R1 = AXBS_0.PORT[7].PRS.R <- Program locks up. No IOVR

unsigned long R2 = AXBS_0.PORT[7].CRS.R <- Program locks up. No IOVR

unsigned long R3 = AXBS_0.MGPCR[7].MGPCR.R <- Works just fine.

I know it should be working, since there are 8. 

AXBS_PORT_tag PORT[8];
AXBS_MGPCR_tag MGPCR[8];

The Reference manual shows that as well.

pastedImage_1.png

I don't know if there is a problem with the Header file, but I have included it.

/* ============================================================================
=============================== Module: AXBS ===============================
============================================================================ */

typedef union AXBS_PORT_PRS_union_tag { /* Priority Registers Slave */
vuint32_t R;
struct {
vuint32_t _unused_31:1;
vuint32_t M7:3; /* Master 7 Priority. Sets the arbitration priority for this port on the associated slave port. */
vuint32_t _unused_27:1;
vuint32_t M6:3; /* Master 6 Priority. Sets the arbitration priority for this port on the associated slave port. */
vuint32_t _unused_23:1;
vuint32_t M5:3; /* Master 5 Priority. Sets the arbitration priority for this port on the associated slave port. */
vuint32_t _unused_19:1;
vuint32_t M4:3; /* Master 4 Priority. Sets the arbitration priority for this port on the associated slave port. */
vuint32_t _unused_15:1;
vuint32_t M3:3; /* Master 3 Priority. Sets the arbitration priority for this port on the associated slave port. */
vuint32_t _unused_11:1;
vuint32_t M2:3; /* Master 2 Priority. Sets the arbitration priority for this port on the associated slave port. */
vuint32_t _unused_7:1;
vuint32_t M1:3; /* Master 1 Priority. Sets the arbitration priority for this port on the associated slave port. */
vuint32_t _unused_3:1;
vuint32_t M0:3; /* Master 0 Priority. Sets the arbitration priority for this port on the associated slave port. */
} B;
} AXBS_PORT_PRS_tag;

typedef union AXBS_PORT_CRS_union_tag { /* Control Register */
vuint32_t R;
struct {
vuint32_t RO:1; /* Read Only */
vuint32_t _unused_30:1;
vuint32_t _unused_24:6;
vuint32_t HPE7:1;
vuint32_t HPE6:1;
vuint32_t HPE5:1;
vuint32_t HPE4:1;
vuint32_t HPE3:1;
vuint32_t HPE2:1;
vuint32_t HPE1:1;
vuint32_t HPE0:1;
vuint32_t _unused_10:6;
vuint32_t ARB:2; /* Arbitration Mode */
vuint32_t _unused_6:2;
vuint32_t PCTL:2; /* Parking Control */
vuint32_t _unused_3:1;
vuint32_t PARK:3; /* Park */
} B;
} AXBS_PORT_CRS_tag;

typedef struct AXBS_PORT_struct_tag {
AXBS_PORT_PRS_tag PRS; /* Priority Registers Slave */
uint8_t PORT_reserved0[12];
AXBS_PORT_CRS_tag CRS; /* Control Register */
uint8_t PORT_reserved1[236];
} AXBS_PORT_tag;

typedef union AXBS_MGPCR_MGPCR_union_tag { /* Master General Purpose Control Register */
vuint32_t R;
struct {
vuint32_t _unused_3:29;
vuint32_t AULB:3; /* Arbitrates On Undefined Length Bursts */
} B;
} AXBS_MGPCR_MGPCR_tag;

typedef struct AXBS_MGPCR_struct_tag {
AXBS_MGPCR_MGPCR_tag MGPCR; /* Master General Purpose Control Register */
uint8_t MGPCR_reserved0[252];
} AXBS_MGPCR_tag;

struct AXBS_tag {
AXBS_PORT_tag PORT[8];
AXBS_MGPCR_tag MGPCR[8];
};

Labels (1)
Tags (2)
1 Reply

411 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

looking into latest device cut I can see that PRS7 and CRS7 are not implemented or accessible for read/write operation.

I expect that they are assigned to HSM module.

pastedImage_2.png

See the screen below. Reading them will result into IVOR1.

pastedImage_1.png

regards,
Peter