Dear NXP Engineers:
I have some questions about the 2 NCFs below , sincerely ask for your help。
Backgrounds :
CPU : MPC 5745B
Specification :MPC5746C_RM_Rev4.pdf
NCF[5] : Configuration error during reset while loading STCU configuration
I assume it happens in the phase3 during reset,In my opinion,there may be 2 reasons that can cause this NCF。
- DCF Recores error :If it happens,Software can do nothing to recover it , the device is unuseable anymore.
- DCF Records are correct, but some problems happen during flash read。
- If it happens,it is possiable to be recovered by a long reset。
- since FCCU configurations are saved in the NVM, if I set the reaction of NCF[5] as long reset,It is able to long reset at once 。
Please kindly correct me if I’m wrong。
I’m also wondering ,If I do nothing when the error occurs ,what will happen?
-Will the CPU continue to excute BIST ,and set a BIST error?
-Or Jump over the BIST ,run the application directly?
-Or hold in the Phase 3?
NCF[8] : Critical fault indication from STCU in case selftest control signals go to wrong condition during user application
What’s the meaning of this error ?Does it mean that the BIST run in the application mode unexpectedly?
Since the online BIST is started by the user application , I’m not sure how the cpu differs the application BIST from shutdown BIST.
What will happen if this error occurs , how shall I resolve it?
Thans a lot for your support.
Best Regrads
Vera