MPC5744P failed to feed watchdog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P failed to feed watchdog

573 Views
chenglei1
Contributor I

Use the watchdog timer for one second, it's normal reset.

Using the follow code to feed watchdog,then keep reset and reset.

Just want to know how to feed the watchdog.

codes as follow:

SWT_0.SR.B.WSC = 0xA602;

SWT_0.SR.B.WSC = 0xB480;

Tags (1)
2 Replies

433 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

If the SWT_CR[SMD] field is 00b, the fixed service sequence mode is selected, which requires writing 0xA602, then 0xB480 to the SWT_SR[WSC] field to service the watchdog. There is no timing requirement between the two writes and the service
sequence logic ignores unlock sequence writes.

Peter

433 Views
chenglei1
Contributor I

Hi,Peter

Thanks for your reply。Although SWT_CR[SMD] field is 00b,use the following code feed watchdog,it still keep reset and reset.

Reference MPC5744P user manual:Invalid access to the SWT causes a system reset if WEN=1

codes as follow:

SWT_0.SR.B.WSC = 0xA602;

SWT_0.SR.B.WSC = 0xB480;

But,I have solved this problem。

Fixed Service Sequence,SWT_CR[SMD] field is 00b。

And use the follow code to feed watchdog:

 SWT_0.SR.R = 0x0000A602;
 SWT_0.SR.R = 0x0000B480;

do as show above,the watchdog is working normally。

0 Kudos