MPC5744P debugger stucked

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744P debugger stucked

1,357 Views
renhaochen
Contributor II

Dear all:

I met some problem when using MULTILINK UNIVERSAL FX to debug our own product which is use MPC5744P as the controller, and it was in S32DS.

When I start debugging, the progress shows 98%, and the console stops with the message below:

"

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00FA0000-00FA0007 ...

"

But with the sample project and source code, this situation doesn't happened in DEVKIT.

Is anybody had met this kind of problem and knows how to fix it?

Thank you.

Tags (2)
4 Replies

994 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

it seems your issue is the same as in the thread below.

https://community.nxp.com/thread/473662 

Please check this thread and eventually send me back the same information. It seems this is about incorrect debugger settings.

Regards,

Martin

367 Views
lzheng
Contributor II

I met exactly the same problem. Replacing with another control board resolved the issue. Therefore, it is not related to the debug setting or firmware issue. 

I need to find out the root cause as this is for production. Any solutions or explanation why it failed? 

0 Kudos

994 Views
yanronglu
Contributor II

Hi Martin:

            I had this problem, too, where the power off while I was programming, and then I had this problem.Can the chip be reused?

0 Kudos

994 Views
renhaochen
Contributor II

Hi Martin:

 

Thank you for replying, but the situation is not as same as that thread

Why cannot programming the mpc5744P? 

Instead, I solved this problem by changing a new MPC5744P micro controller.

I assume that maybe the old one is not functionally OK.

0 Kudos