I am using document "AN4365 Qorivva MPC56xx Flash Programming Through Nexus JTAG.pdf " to entry debug mode. MPC56xx device is ok, however, MPC5744P is fail.
I review MPC5744P Reference Manual. I don't kown which one of ACCESS_AUX 5-bit JTAG instructions is right. It seem 6-bit is right
code below:
JTAG_IR_Scan(0x1, 5); //5 bit
rdata = JTAG_DR_Scan_Read(0x0,32); //0x39b4501d jtag id is ok
JTAG_IR_Scan(0x1A, 6); //6 bit
rdata = JTAG_IR_Scan(WRITE_RS|OCR, 10); //0x241 read OSR is ok
JTAG_DR_Scan(0x5,32); // Set the OCR[DR] and OCR[WKUP] bits
SET RESET=1;
DelayMs(100);
rdata = JTAG_IR_Scan(READ_RS|BYPASS, 10); //0x221 read OSR is error
if(rdata!=0x209) Fail();
1) Which one of ACCESS_AUX 5-bit JTAG instructions? I try 0x10,0x17,0x18,0x1a,0x1e
2) Only OSR return 0x209 is right, and entry debug mode, Why I test return 0x221 Halt mode ?
已解决! 转到解答。
Hi,
It’s necessary to use ACCESS_AUX_LSM (code 0b11010) on devices which has two cores running in lock step mode.The rest should be the same like on MPC56xx devices.
https://community.nxp.com/docs/DOC-332727
Regards,
Lukas
Hi,
It’s necessary to use ACCESS_AUX_LSM (code 0b11010) on devices which has two cores running in lock step mode.The rest should be the same like on MPC56xx devices.
https://community.nxp.com/docs/DOC-332727
Regards,
Lukas