Hi,
I am working with MPC5744P with the e200z4 processors using the S32DS version 2.1.
Application - Industrial (Safety critical IEC61508)
Since the SDK was not safety certified, it was suggested to used the ISO26262 MCAL drivers, which was created for the AUTOSAR project [1]. But in its integration manual, it is mentioned that I have to use Tresos tool to modify and generate MCAL component configuration [2]. Does it mean that I cannot use the Processor Export tool for generating configurations here when using the ISO26262 MCAL package. Could you please clarify? and also on how to use the ISO MCAL package in the non-AUTOSAR environment?
[1] https://community.nxp.com/t5/MPC5xxx/Safety-certification-for-the-gcc-compiler-in-S32DS-for-power/m-...
[2] AUTOSAR_MCAL_SPI_IM Section 5.3 and also AUTOSAR_MCAL_SPI_UM Section 3.6.2 pdfs
Thank you