MPC5744P IVOR1 exception when accessing16 bits of DMEM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P IVOR1 exception when accessing16 bits of DMEM

1,430件の閲覧回数
ilya_kogan
Contributor I

With stack in the local memory there is an exception when accessing 16-bit local variables:

j is a 16-bit variable.

r31 = 0x50800748

 93 int argc=0;
40007fa0: se_li r7,0
40007fa2: se_stw r7,44(r31)
ee_u16 j=0;
40007fa4: se_li r7,0


40007fa6: se_sth r7,10(r31)


e_u16 num_algorithms=0;
40007fa8: se_li r7,0
40007faa: se_sth r7,12(r31)
ee_s16 known_id=-1;
40007fac: se_bmaski r7,0
40007fae: se_sth r7,14(r31)
ee_s16 total_errors=0;
40007fb0: se_li r7,0
40007fb2: se_sth r7,16(r31)
ee_u16 seedcrc=0;

MEMORY
{

SRAM : org = 0x40000000, len = 384K

local_dmem : org = 0x50800000, len = 64K
}

.stack (NOLOAD) : ALIGN(16)
{
__HEAP = . ;
PROVIDE (_end = . );
PROVIDE (end = . );
. += __HEAP_SIZE ;
__HEAP_END = . ;
_stack_end = . ;
. += __STACK_SIZE ;
_stack_addr = . ;
__SP_INIT = . ;
. += 4;
} > local_dmem

0 件の賞賛
返信
2 返答(返信)

1,260件の閲覧回数
asdqwe
Contributor I

Hello,

I met the same problem, has issue been sloved?

Thank you.

0 件の賞賛
返信

1,260件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, it'll be apparently because of 32-bit data ECC granularity on DMEM memory. DMEM needs to be initialized by 32-bit writes to completely define ECC code for data unit. Then less than 32-bit access can be performed.

0 件の賞賛
返信