Hi,
I meet a ADC analog watchdog problem ,I want to make the result of analog watchdog monitoring ADC conversion in the threshold area I set.
If it is not in the range, the interrupt function is used to process the data . But now the ADC_0.WTISR.B.WDG1H or ADC_0.WTISR.B.WDG1L position is 1, and the program does not interrupt
follow is my setting
ADC_Init(0,CH5Smask,0,SCAN); //ADC0 clk is 80MHZ enable adc0_CH5 scan mode,
ADC_SetThldForChannel(0,5,1); //setting ADC0 THreshold register 1 add to channel5
ADC_SetThldRegister(0,1,0x800,0xAAA,0x0C); //enable wdg1H and WDG1L setting Threshold
ADC_StartNormalConversion(0,CH5Smask); //start conversion
for(;;) {
volt = ADC_GetChannelValue(0, 5); //auto clear flag
volt = volt*3300/4095;
if(ADC_0.WTISR.B.WDG1H ==1) //check interrupt flag
cnt++;
if(ADC_0.WTISR.B.WDG1L ==1) //check interrupt flag
cnt++;
}
void ISR498_ADC0_WD(void) //WD interrupt deal
{
volatile uint32_t volt = 0;
volt = ADC_GetChannelValue(0, 5);
volt = volt*3300/4095; //将结果放大1000倍
ADC_ClearThldFlags(0);
}