MPC5744 schematic review

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744 schematic review

1,247 Views
hansonhe
NXP Employee
NXP Employee

Hello,

Could you help review attached MPC5744 mini system schematic? Thanks.

0 Kudos
1 Reply

1,161 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Hanson,

1. There shouldn't be R268.
2. VPP_TEST can be connected directly to GND without pull down resistor.
3. And to be meticulous - AN5267 recommends to use 10uF and 100nF on VDD_HV_PMU but there's 10uF and 10nF in the schematic.

Regards,

Lukas

0 Kudos