MPC5744 interrupt stuck at "IVOR1_Vector() at 0xfa2010"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744 interrupt stuck at "IVOR1_Vector() at 0xfa2010"

1,351 Views
pizzburg
Contributor I

I'm using MPC5744, it works fine for a long time. But today something just go wrong, when PIT triggerd interrupt, the process stuck!   From debugging I find that pc stuck at address 0x00FA2010,   this is an adress so called "IVOR1_Vector". it is someting relative to interrupt process.    

The datasheet said in software vector mode, interrupt should go to "IVOR4_Vector", but not "IVOR1_Vector". 

I did some mod on the INTC code, sometimes it also stuck at 0x00FA2060, whitch is "IVOR6_Vector", such as when I change it to "Hardware vector mode."

Before today, everything just goes fine. I don't know why this happens.  

Who can tell why the interrupt goes to  0x00FA2010 or 0x00FA2060? 

Thanks!    

Waiting for an answer.

pastedImage_1.png

pastedImage_2.png

Noticed:    No source available for "IVOR1_Vector() at 0xfa2010" 

1 Reply

956 Views
1060111312
Contributor II

I also meet this problem.And have you solved the problem?

0 Kudos
Reply