MPC5744,XOSC initialize start-up phase of the waveform problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5744,XOSC initialize start-up phase of the waveform problem

1,570 Views
DELPHI_Eric
Contributor III

152429_152429.png加代码Q9波形 - 副本.png

Here is the code I use,according to DEMO.

void g_v_MCModeInit(void)

    vuint32_t      temp,timer;

 

    /* Disable Software Watchdog (SWT) */

    SWT_0.SR.R                        = 0xc520;

    SWT_0.SR.R                      = 0xd928;

    SWT_0.CR.R                      = 0x8000010A;

 

    /* Clear all "Functional Event Status reset sources" to avoid staying in SAFE mode */

    MC_RGM.DES.R = 0xFFFFFFFF;               //write 1 to clear dest reset events

    MC_RGM.FES.R = 0xFFFFFFFF;               //write 1 to clear func reset events

    MC_ME.ME.R = 0x000005FF;    //enable all modes

 

 

    XOSC.CTL.B.OSCM = 0x1;       //Without this code, the start-up phase of the waveform more unstable

   XOSC.CTL.B.EOCV = 0x80;        //This code with or without observation oscilloscope waveforms found no effect

 

 

    // Enable the EXTAL clk

 

    MC_ME.DRUN_MC.B.XOSCON=1;

 

    /* RE enter the drun mode, to update the configuration */

    MC_ME.MCTL.R = 0x30005AF0;                       /* Mode & Key */

    MC_ME.MCTL.R = 0x3000A50F;                /* Mode & Key inverted */

    while(MC_ME.GS.B.S_MTRANS == 1);                /* Wait for mode entry to complete */

    while(MC_ME.GS.B.S_CURRENT_MODE != 0x3);       /* Check DRUN mode has been entered */

    /* Wait for clock to stabilize */

    while(!MC_ME.GS.B.S_XOSC);

Labels (1)
2 Replies

1,243 Views
liujinhang
Contributor III

Any body help me?

0 Kudos
Reply

1,243 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have assigned similar question from different customer, now waiting for factory response. However it seems it is common behavior of this device.