MPC5676R Internal Temperature Sensor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5676R Internal Temperature Sensor

1,011 Views
nicklabianco
Contributor I

The datasheet for this device states that the accuracy is +/- 10 degrees Celsius. Is this true if the internal calibration constants are used or can you obtain a better accuracy when using the internal calibration parameters?

Labels (1)
0 Kudos
Reply
1 Reply

933 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

These internal sensors are typically quite imprecise, thus +/-10 °C is valid even it is calibrated in accordance to reference manual. Of course accuracy will be better than +/-10 °C as these values are corner cases.

0 Kudos
Reply