MPC5675K: How to program the user reserved space of the test sector

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5675K: How to program the user reserved space of the test sector

615 Views
BG
Contributor II

Hello!

I would like to program custom records into the user reserved space of the test sector (addresses 0x40_3D00–0x40_3DE7 as per p.207 of the MPC5675K reference manual) using a Trace32 debugger.

I tried the following flash procedure:

FLASH.Create 1. 0x00400000++0x03fff TARGET Quad 0.

FLASH.TARGET E:0x40000000 E:0x40004000 0x1000 ~~/demo/powerpc/flash/quad/c90fl567xk.bin /STACKSIZE 0x0200 /DualPort

Flash.unlock ALL

Flash.Program 1.

Data.LOAD.Binary "test_record.bin" 0x403D00 /Quad

;Complete flash programming
flash.program 1.

The test record has a size of 8 bytes.

However, this fails with the error message "Flash programming error around address SF:0x403D00--0x403E8F" when the Data.LOAD.Binary statement is executed.

Is there any option I have to set to be able to write to this area or is there any operation I have to perform before writing to it?

Thank you,
Bernd

0 Kudos
Reply
1 Reply

601 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is needed to have set PEAS bit in the flash MCR register. I am not sure if TRACE32 has command for it, but write to specific address may be done by TRACE32 as well.

davidtosenovjan_0-1698159549914.png

 

0 Kudos
Reply