MPC5674F Unable to capture an external interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5674F Unable to capture an external interrupt

1,998件の閲覧回数
volpato
Contributor I

I'm having trouble setting MPC5674F to capture an external interrupt. I tried to adapt the examples from AN2865 Qorivva Simple Cookbook and also tried to follow the steps dictated in MPC5674F Reference Manual, but without success.

My goal is to capture an interrupt via signal EMIOS14_IRQ0_GPIO193 using INTC in HW vector mode. (I also tried SW vector mode too, but couldn't make it work).

Could you please provide an example for this scenario?

ラベル(1)
0 件の賞賛
返信
1 返信

1,523件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Try to see following example, it is the same principle:

Example MPC5606B SIUL External interrupt

0 件の賞賛
返信