MPC5674F Bootload

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5674F Bootload

1,238 Views
pyi285
Contributor II

Can someone explain me the code or method to bootloader the MPC5674F chip?

The chip I have is SPC5674FMVVS chip

 

#MPC5674F #bootloader #SPC5674

0 Kudos
Reply
4 Replies

1,229 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @pyi285 

We provide Rappid bootloader which can use either UART or CAN (per release notes - only UART in case of MPC5674F). It uses BAM serial boot mode. Notice that we do not provide source codes, it cannot be modified:

https://www.nxp.com/webapp/Download?colCode=RAPPID_BOOTLOADER_UTILITY&appType=license

To start this bootloader, it is necessary to reconfigure BOOTCFG pins in order to start BAM serial download. If it is not suitable for your application, it’s necessary to use flash resident bootloader.

 

If you are interested in flash resident bootloader, attached is a draft of application note:

https://community.nxp.com/servlet/JiveServlet/download/427962-1-279359/bootloader.zip

It’s written directly for MPC5634M, software is working. It can be used as a starting point to develop own solution. It’s necessary to use these SSD flash drivers:

http://www.nxp.com/lgfiles/Qorivva/MPC5674F_C90FL_SSD_DRV.exe

 

Just in case, this is updated and published version for MPC57xx devices (software is written for MPC5748G):

http://www.nxp.com/assets/documents/data/en/application-notes/AN5319.pdf

http://www.nxp.com/assets/documents/data/en/application-notes-software/AN5319SW.zip

 

And if you are looking for out of box solution, you can ask Vector (or other SW vendors) for help:

https://www.vector.com/int/en/products/products-a-z/embedded-components/flash-bootloader#

Regards,

Lukas

0 Kudos
Reply

1,129 Views
pyi285
Contributor II

Can you write the Bootloader code used with the SPC5674FF3MVV3 Chip?

0 Kudos
Reply

1,123 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

This is not a service provided by our free online technical support. You can request a solution from our paid engineering services:

https://www.nxp.com/support/support/nxp-engineering-services:SW-SUPPORT

Regards,

Lukas

0 Kudos
Reply

1,063 Views
pyi285
Contributor II
I am sorry But I don't have enough time, so I need a quick answer and an accurate code. I urgently need a bootloader code related to the MPC5674F chip I am using.
If you can't write the code, can you elaborate on the address or register that needs to be changed?
please i need a lot

It is difficult to understand the present
0 Kudos
Reply