HELLO,all,
WHEN I use the CW10.6 FOR debugging MPC5645, I encountered such two errors. The code is compiled with no error. Does anyone know how to solve this?
It seems like the function _declspec(vle_on) can’t start up, related to core 1 started failed.
YES,THE code is compiled well,but can't run successfully,I attach the CDT build console INFO below. I guess it is BECAUSE the CW10.6 I use now is configued somewhere wrong. IT can‘t be compatable to the character '@', so IT cant reach to de correct flash memory.
Starting 3rd party flash programming...
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : STARTUP, Entry : SPECIFY_NETWORKCARD_ENABLED, Value : 0, R) => DI_ERR_NONFATAL
INF: Copyright 2012 P&E Microcomputer Systems,Inc.
INF: Command Line :"D:\SoftwareTools\CW10.6\CW MCU v10.6\eclipse\..\MCU\bin\de.exe" -noni -language en -ORBendPoint giop:tcp:127.0.0.1: -ORBtraceLevel 0
INF: CMD>RE
INF: Initializing.
INF: Target has been RESET and is active.
INF: CMD>CM D:\SoftwareTools\CW10.6\CW MCU v10.6\MCU\bin\Plugins\support\EPPC\gdi\P&E\freescale_mpc5646c_1x32x768k_lcflash.pcp
INF: Initializing.
INF: Initialized.
INF: ;version 1.03, 09/28/2012, Copyright P&E Microcomputer Systems, www.pemicro.com [5646x_3072k_LCFlash]
INF: ;device Freescale, MPC5646C, 1x32x768k, desc=LCFlash
INF: ;begin_cs device=$30000000, length=$00300000, ram=$00300000
INF: Loading programming algorithm ...
INF: Done.
INF: CMD>EM
INF: Erasing.
INF: Module has been erased.
INF: CMD>PM
INF: Programming.
INF: Processing Object File Data ...
INF: .
INF: Programmed.
INF: CMD>VC
INF: Verifying object file CRC-16 to device ranges ...
INF: block 00000000-00000007 ...
INF: Ok.
INF: block 00000010-000004D7 ...
INF: Ok.
INF: block 00010000-000100F3 ...
INF: Ok.
INF: block 00010100-000101A3 ...
INF: Ok.
INF: block 00020000-000200F3 ...
INF: Ok.
INF: block 00020100-000201CF ...
INF: Ok.
INF: block 00040000-000536B3 ...
INF: Ok.
INF: block 000536B8-0005396B ...
INF: Ok.
INF: block 00054000-0005471F ...
INF: Ok.
INF: Checksum Verification Successful. (Cumulative CRC-16=$2582)
INF: CMD>RE
INF: Initializing.
INF: Target has been RESET and is active.
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : DEFAULT, Entry : MODE27, Value : Unknown Processor, R) => DI_ERR_NONFATAL
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : Unknown Processor, Entry : REGISTERMASK, Value : *.reg, R) => DI_ERR_NONFATAL
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : Unknown Processor, Entry : RESETADDR, Value : -1007091700, R) => DI_ERR_NONFATAL
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : Unknown Processor, Entry : WATCHADDR, Value : 0, R) => DI_ERR_NONFATAL
GDI: Mtwks Callback(MTWKS_CB_PROJECTACCESS, Section : Unknown Processor, Entry : FLASHALG, Value : , R) => DI_ERR_NONFATAL
INF: WARNING - NO RESET SCRIPT FILE HAS BEEN CONFIGURED TO RUN!!!
INF: TO MODIFY THE RESET SCRIPT SETTINGS, USE THE FOLLOWING MENU OPTION:
INF: CONFIGURATION -> AUTOMATED SCRIPT OPTIONS