MPC5643L Test flash memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5643L Test flash memory

692 次查看
Pat
Contributor III

Hi,

Do you have an example or real values for the fields PART ID 1 H/L and PART ID2  of the Test flash memory of MPC5643L  ?

RM rev10 :

pastedImage_1.png

My Current Test flash memory values :

pastedImage_2.png

Best regards,

Pat

标记 (2)
0 项奖励
2 回复数

590 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, I would guess it is only related to KGD (Known Good Die). As all KGD references has been removed, apparently it is not a option and these field don't need to be programmed in the factory.

pastedImage_1.png

0 项奖励

590 次查看
Pat
Contributor III

Hi davidtosenovjan‌,

So, these fields should be also removed from the last MPC5643LRM  Rev10, Table 23-24. Test flash information.

Thank you.

BR,

Pat

0 项奖励