Hi petervlna,
I have defined a -wx(read not allowed) region for CoreZ4d/Nexus master with MPU module in order to create an IVOR1 exception when the core read data in this region.
The IVOR1 occurs as expected, then I clear the MCSR register with the following code :
void IVOR1_Exception_Handler(void){
uint32_t mcsr = __MFSPR(572);
__MTSPR(572, mcsr);
/* Enables region 2 to grant Core Z4D_0 read permission */
(void)SMPU_DRV_EnableRegion(SMPU_0, 2U, true);
}Please have a look on attached intc_sw_handlers file and let me know your changes or comments.
Best regards,
Pat