MPC5643L: Config shadow memory to bypass self test(LBIST, MBIST)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5643L: Config shadow memory to bypass self test(LBIST, MBIST)

913 Views
rajakumaranazha
Contributor II

Hello,

We are using MPC5643L daughter board with MC33908 mother board for our evaluation testing.

codewarrior version:  "CW for MPC55xx and MPC56xx 2.10".

We could successfully power up the evaluation board in LSM as well as in DPM by updating the shadow flash memory.

We are testing the BIST feature available in MPC5643L. With default configuration in shadow memory, it executes the BIST(LBIST & MBIST) and the corresponding status are available in the relevant registers.

Now, we would like to bypass the self test by writing the below code in the shadow memory by using algorithm "Freescale_MPC5643L_1x32x4k_Shadow_Blk.pcp" & application "cw_progppcnexus.exe"

pastedImage_4.png##@

But even with above configuration code, the self test is being executed and status available as "Self-test complete" .

Can anyone help us with configuration procedure or additional settings required if any?

Labels (1)
Tags (4)
0 Kudos
Reply
1 Reply

749 Views
petervlna
NXP TechSupport
NXP TechSupport
0 Kudos
Reply