Hello All,
I am trying to run AUTOSAR on MPC5634M with NXP MCAL&OS with EB Tresos studio.
For this chip, NXP supports AUTOSAR v 3.0.
I have two questions:
1) I am using "Tresos Studio " Release ver 2009.a build number: b090820-1820.
OS Ver: Freescale AUTOSAR OS/MPC56xxAM v.3.0 RTM, build 3.0.35.
I have also added the patch "OSMPC56xxAM_3_0_35_patch1"
I receive the following error (attached image) after importing the sample project: "os_sample_sc1" located in "\AUTOSAR\os_freescale_mpc56xxAM\os_ts\eclipse\workspace" to Tresos studio and running "Generate Project".
I am running on windows 7 64 bit system. Is a 32bit OS required for the configuration?
2) The MCAL provided for the same chip is "AUTOSAR MPC563XM MCAL3.0 swv: 2.0.0 RTM". But this MCAL version expects "Tresos Studio ver 2010". But as stated in qn. 1), OS expects "Tresos Studio " Release ver 2009.
How can i configure the entire project in this case, when there is a conflict in versions as seen here.
Any help to address the above questions and get the configurator to work is appreciated.
Your Sincerely,
Arjun
已解决! 转到解答。
Hello Arjun,
to the questions:
1) I see the same error if generating on Windows 10 64-bit. The error is reported because by default on 64-bit operating system there is used 64-bit java. The MPC5634M Autosar OS supports only 32-bit java so to generate it is needed to install the 32-bit java. Then it is also needed to put the path to the 32-bit java to the PATH environmental variable so that it will be found while generating in Tresos.
The version of java can be checked with command java -version executed from command prompt:
c:\>java -version
java version "1.8.0_201"
Java(TM) SE Runtime Environment (build 1.8.0_201-b09)
Java HotSpot(TM) 64-Bit Server VM (build 25.201-b09, mixed mode)
On my windows 10 computer there is used 64-bit java by default (see the string “64-Bit Server VM”).
I have modified the path variable with the following command to add path to 32-bit java:
c:\>path="c:\Program Files (x86)\Java\jre1.8.0_201\bin";%path%
So then the java version reported is 32-bit (string “Client VM”) as shown here:
c:\>java -version
java version "1.8.0_201"
Java(TM) SE Runtime Environment (build 1.8.0_201-b09)
Java HotSpot(TM) Client VM (build 25.201-b09, mixed mode)
After this I open the Tresos with this command (still in the same command prompt window):
c:\>c:\EB\tresos2010.a.sr4\bin\tresos_gui.exe
and I can generate correctly without any error.
If you prefer you can just add the path to the 32-bit java to your PATH environmental variable so that 32-bit java would be always used (but be careful that this could impact other programs that might require 64-bit java).
2) There can be used the newer version (Tresos 2010.sr4) to configure both MCAL and OS. See the MCAL sample application (located in c:\Freescale\AUTOSAR\MPC563XM_MCAL3.0_RTM_2.0.0_signed\MPC563XM_MCAL3.0_RTM_2.0.0_Integration_Application) where both MCAL and OS are integrated within one project. See here the screenshot from Tresos:
Best Regards,
Frantisek
Hello Arjun,
to the questions:
1) I see the same error if generating on Windows 10 64-bit. The error is reported because by default on 64-bit operating system there is used 64-bit java. The MPC5634M Autosar OS supports only 32-bit java so to generate it is needed to install the 32-bit java. Then it is also needed to put the path to the 32-bit java to the PATH environmental variable so that it will be found while generating in Tresos.
The version of java can be checked with command java -version executed from command prompt:
c:\>java -version
java version "1.8.0_201"
Java(TM) SE Runtime Environment (build 1.8.0_201-b09)
Java HotSpot(TM) 64-Bit Server VM (build 25.201-b09, mixed mode)
On my windows 10 computer there is used 64-bit java by default (see the string “64-Bit Server VM”).
I have modified the path variable with the following command to add path to 32-bit java:
c:\>path="c:\Program Files (x86)\Java\jre1.8.0_201\bin";%path%
So then the java version reported is 32-bit (string “Client VM”) as shown here:
c:\>java -version
java version "1.8.0_201"
Java(TM) SE Runtime Environment (build 1.8.0_201-b09)
Java HotSpot(TM) Client VM (build 25.201-b09, mixed mode)
After this I open the Tresos with this command (still in the same command prompt window):
c:\>c:\EB\tresos2010.a.sr4\bin\tresos_gui.exe
and I can generate correctly without any error.
If you prefer you can just add the path to the 32-bit java to your PATH environmental variable so that 32-bit java would be always used (but be careful that this could impact other programs that might require 64-bit java).
2) There can be used the newer version (Tresos 2010.sr4) to configure both MCAL and OS. See the MCAL sample application (located in c:\Freescale\AUTOSAR\MPC563XM_MCAL3.0_RTM_2.0.0_signed\MPC563XM_MCAL3.0_RTM_2.0.0_Integration_Application) where both MCAL and OS are integrated within one project. See here the screenshot from Tresos:
Best Regards,
Frantisek
Hello Frantisek,
Thanks a lot for the solution.
It has worked perfectly well and now I am able to generate code from Tresos studio.
Thanks a lot for taking the time out to answer this query in detail.
Good day to you.
Arjun.