Hi,
We have chosen the mpc5606s for mid range instrumental cluster in two and three wheeler. Now need some clarification on,
1. Graphics - will mpc5606s support LVGL libraries, if not suggest which graphics libraries will be supporting for designing the instrumental in mpcs5606s.
2. Display - In datasheet it mentioned it can support up to WVGA (800X480) and in some part of the documents it is mentioned it can support only WQVGA(480X260). Which resolution it supports the maximum.
Thanks,
Vivishekh
HI, here you may find the answer:
Thanks. Kindly clarify point 1,
Does MPC5606s supports LVGL libraries? We use XPC560SKIT evb. If LVGL is not supported then what are the alternatives .
No, it is not supported by MPC5606S.
Here is the list of supported platforms:
Graphics library for MPC5606S can be shared to customer as per NDA basis.
Please create new case with the question according procedure below:
If vector graphic is required, consider using of MPC5645 device, having OpenVG accelerator:
https://community.nxp.com/t5/MPC5xxx/mpc5645s-can-use-openvg/m-p/640867
... or some newer device