MPC5606B startertrak board max input voltage for port pins

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5606B startertrak board max input voltage for port pins

跳至解决方案
1,877 次查看
sundar19
Contributor III

Hi,

I am using mpc5606b startertrak dev board . I have attached external transceivers TJA1050 with the CAN bus pins. I have supplied 5V to transceivers and thus the same logic voltage is applied to CAN port pins of mpc5606b. Can mpc5606b pins take 5V input? Will it damage the pins? 

0 项奖励
回复
1 解答
1,862 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.

The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant.

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
5 回复数
1,863 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.

The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant.

Regards,

Lukas

0 项奖励
回复
1,855 次查看
sundar19
Contributor III

You saying that if I power up mpc5606b with 3.3V , then its pins arent 5V tolerant? 
thank you

0 项奖励
回复
1,849 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, you can find in the datasheet:

lukaszadrapa_0-1621596721976.png

 

Regards,

Lukas

0 项奖励
回复
1,850 次查看
sundar19
Contributor III

Thank you

0 项奖励
回复
1,858 次查看
sundar19
Contributor III

Thank you so much

0 项奖励
回复