MPC5606B startertrak board max input voltage for port pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5606B startertrak board max input voltage for port pins

Jump to solution
1,746 Views
sundar19
Contributor III

Hi,

I am using mpc5606b startertrak dev board . I have attached external transceivers TJA1050 with the CAN bus pins. I have supplied 5V to transceivers and thus the same logic voltage is applied to CAN port pins of mpc5606b. Can mpc5606b pins take 5V input? Will it damage the pins? 

0 Kudos
Reply
1 Solution
1,731 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.

The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
5 Replies
1,732 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

TRK-MPC5606B is supplied by 5V only, it's not configurable to 3.3V. So, there's no problem, you can connect a transceiver supplied by 5V.

The microcontroller itself supports both 3.3V and 5V supply voltage.But if 3.3V is used, the GPIO pins are not 5V tolerant.

Regards,

Lukas

0 Kudos
Reply
1,724 Views
sundar19
Contributor III

You saying that if I power up mpc5606b with 3.3V , then its pins arent 5V tolerant? 
thank you

0 Kudos
Reply
1,718 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Yes, you can find in the datasheet:

lukaszadrapa_0-1621596721976.png

 

Regards,

Lukas

0 Kudos
Reply
1,719 Views
sundar19
Contributor III

Thank you

0 Kudos
Reply
1,727 Views
sundar19
Contributor III

Thank you so much

0 Kudos
Reply