I just read about the included Boot Assist Module in MPC5606B. I understand that I have to set the FAB and ABS pins accordingly to disable booting from internal flash and make use of the Boot Assist Module instead.
Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?
Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?
For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?
Thank you very much in advance!
解決済! 解決策の投稿を見る。
Hi,
- Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?
- Yes.
- Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?
- Yes:
- For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?
- Yes:
Regards,
Lukas
Hi,
- Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?
- Yes.
- Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?
- Yes:
- For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?
- Yes:
Regards,
Lukas