MPC5604B can not enter the interrupt service routine

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604B can not enter the interrupt service routine

1,401 Views
jeffcharles
Contributor III

Hi,

PIT channel 0 can work in the debug mode, the status of  related registers are shown in the attachments. But it can not enter the ISR, my configurations and ISR about INTC like this, the whole codes are in the attachments.

void intc_init(void)
{    
    /* Initialization of the exception handlers and INTC */
    EXCEP_InitExceptionHandlers();
    INTC_InitINTCInterrupts();
    
    /* Enable interrupts in INTC:
     * PIT channel 0
     *
     */
    INTC_InstallINTCInterruptHandler(pit_ch0_isr, 59, 0);    /* PIT channel 0 priority: 0 */
    
    /* Lower current priority - to enable INTC to process interrupts */
    INTC.CPR.R = 0x0;
}


/*    
 *    PIT channel 0 interrupt handler
 */
void pit_ch0_isr(void)
{
    PIT.CH[0].TFLG.R = 0x1;
    SIU.GPDO[0].B.PDO = ~ SIU.GPDO[0].B.PDO;
}

Please help me to solve the problem,thanks!

Labels (1)
Tags (2)
2 Replies

1,230 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

You have to have PIT interrupt priority other then 0 if you want to trigger IVOR4 (external interrupt).

pastedImage_1.png

Peter

1,230 Views
jeffcharles
Contributor III

Hi Peter,

Thank you! The problem has been solved.

0 Kudos