¿MPC5604B_M07N  vs MPC5604B_M27V ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

¿MPC5604B_M07N  vs MPC5604B_M27V ?

1,752 Views
pvarela
Contributor II

What are the differences between MPC5604B_M07N  and MPC5604B_M27V derivatives?

 

I have XPC560B 100LQFP and XPC560B 144LQFP. At the begining I was working with 144 ( I was using MPC5604B_M27V MCU in CW project wizard, but I don't now why...) but now I need to work with 100, and I don't know if I need change that.

 

Thank you.

Labels (1)
0 Kudos
1 Reply

1,028 Views
pvarela
Contributor II

I received this explanation from Freescale support:

"...

The difference is in mask set and their errata. But the mask 07N has never been produced so you can omit this option. I will inform CodeWarrior to remove it.

You should select mask set M27V and everything will be OK.

The mask set defines internal circuitry => errata list. It has no influence on defined features defined by reference manual and data sheet...."